Skip to main content
Renesas Electronics Europe - Knowledgebase

What substitutes are available for transistors 2SA1005 and 2SC945?

Latest Updated:02/01/2008


Transistors 2SA1005 and 2SC945 are shown in the application circuit example in the Data Sheet of the uPD3747 in the stage following the Vout pin. The distributor I contacted said that these products were phased-out products and were not available.
What substitutes are available?


The 2SA1461 may be substituted for the 2SA1005 and the 2SC1623A for the 2SC945, but the package as well as some of the ratings and characteristics differ. See the Data Sheet for details.
Suitable Products
  • Was this article helpful?