Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 Repeatedly Download Image

Last Updated:06/01/2017

Question:

I cannot repeat for the process to download the image, as reference in the Getting Started Manual on page 21. How can I do this?

Answer:

The only thing you have to do at this stage is to re-write the descriptor file "174_1234_01upd.dat" for the target image download as described before. The TFTP server takes this descriptor file and downloads the correct image as set in the descriptor file.
Before you can use the "TPS_UpdaterTarget" and "TPS_Target" images, you have to generate them as described on page 18 in the TPS-1 Starter Kit Getting Started Manual (R21UT0221ED0100, Rev. 1.00).
Suitable Products
TPS-1
  • Was this article helpful?