Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What happens if address signal is changed in SRAM writing operation?

Latest Updated:03/16/2012

Question:

If the address signal is changed during an asynchronous SRAM writing operation (CS pin and WE# are enabled), what will happen?

Answer:

As specified in the datasheet, an address setup time and a write recovery time of more than 0 ns are required. Incorrect writing may occur if this regulation is not obeyed. Please never perform an address signal change during a writing operation.
Suitable Products
Power MOSFETs for General Switching
Power MOSFETs for Automobile use
Asynchronous SRAM