Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can programming be done from flash programmer with crystal resonator?

Latest Updated:12/01/2011

Question:

Can programming be done from the flash programmer with a crystal resonator mounted on the target system (connected to X1, X2)?

Answer:

Yes, programming is possible regardless of whether there is a crystal resonator mounted on the target board or not.
Suitable Products