Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Will cache memory referred and rewritten if address is in cache area?

Latest Updated:03/24/2009

Question:

In DMA transfers, if a designated address is in the cache effective area, will a cache memory be referred and rewritten?

Answer:

No, it is impossible to refer and rewrite a cache memory by DMA transfers.
If a transfer is performed to the external memory designated in the cache effective area by the DMAC, please secure the coherency of the cache memory and the external memory by software.
Suitable Products
SH7700 Series
SH7729R
SH7727
SH7709S
SH7706
SH7705