Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which functions are allocated to the multiplexed pins in boot mode?

Latest Updated:09/09/2011

Question:

Which functions are allocated to the multiplexed pins in boot mode?

Answer:

The following functions are allocated to the pins in boot mode.

・PA4/A4/IRQ2/TXD1 pin: TXD1
・PA3/A3/IRQ1/RXD1 pin: RXD1
・Other pins : initial function in "MCU extension mode2".

For the allocated pin function set in On-Chip ROM Enabled mode, please see "Table 17.11 SH7149 Pin Functions in Each Operating Mode (2)" in "SH7146 Group User's Manual: Hardware".

Suitable Products
SH7146, SH7149