Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Should I set TIOR_5 according to table TIORU_5, TIORV_5, and TIORW_5?

Latest Updated:09/11/2012

Question:

When using the MTU2 external pulse width measurement function, without relation to the combination with the complementary PWM mode, should I set the TIOR_5 register according to the table "TIORU_5, TIORV_5, and TIORW_5 (channel 5)" (Table 11.28 for the SH7286 Hardware manual)?

Answer:

Without relation to the combination with the complementary PWM mode, settings according to the table "TIORU_5, TIORV_5, and TIORW_5 (channel 5)"  (Table 11.28 for the SH7286 Hardware manual) can be made.
Suitable Products
SH7285, SH7286
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7124, SH7125
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086