Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it possible to turn the cache OFF in the specific address space?

Latest Updated:03/25/2009

Question:

Is it possible to turn the cache OFF in the specific address space?

Answer:

Please use P2 area when using with cache OFF because cache is disabled in P2 area within the address spaces of SH-3 and SH3-DSP, and use P0 area when using with cache ON because cache is enabled in P0 area.
Suitable Products
SH7700 Series
SH7729R
SH7727
SH7720
SH7709S
SH7706
SH7705
SH-Ether