Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to set pins not to output signals in changing input to output?

Latest Updated:03/23/2009

Question:

When changing input port into output port in the pin setting,

how should we set the pins not to output an unexpected signal?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
SH7018
SH7011