Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How many PWM can you output from the MTU on SH1/2 ?

Latest Updated:03/26/2009

Question:

How many PWM can you output from the MTU on SH1/2 ?

Answer:

As long as you can accept using the same carrier frequency it is possible to synchronise the timers on the MTU to provide up to 12 channels of PWM. This is achived using channels 0..2 in PWM mode 2 and channles 3..4 in PWM mode 1. PWM mode 2 provides 1 PWM output per compare match and PWM mode 1 provides 1 output for a p[air of compare matches. Ie. 4 + 2 + 2 + (4/2) + (4/2) = 12. The SH1 ITU can provide 5 PWM outputs as only PWM mode 2 is supported.

Suitable Products
SH7144 Series
SH7047 Series
SH7046 Series
SH7040 Series