Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

FPU instruction supported by SH-2E is also supported by SH-2A?

Latest Updated:03/23/2009

Question:

FPU instruction supported by SH-2E is also supported by SH-2A?

Answer:

SH-2A has the lineup in two kinds of CPU cores such as "SH-2A" and "SH2A-FPU".

"SH-2A" doesn't have the instruction related to FPU of "SH-2E" though "SH2A-FPU" supports "SH-2E" instruction.

Meanwhile, SH7206 is a product with on-chip CPU core of "SH-2A".

Suitable Products
SH7206