Skip to main content
Renesas Electronics Europe - Knowledgebase

Does the flash memory version have I2C Bus Interface function too?

Latest Updated:03/25/2009


SH7144/SH7145 Groups have an optional I2C Bus Interface function. Does the flash memory version have it too?


The flash memory version and ROM less version of SH7144/SH7145 Groups include the I2C Bus Interface function.
For the mask ROM version, the I2C Bus Option needs to be specified at the time of ROM ordering.
Suitable Products
SH7144, SH7145