Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can CPU processing keep running when DMAC/DTC is using internal bus?

Latest Updated:03/21/2012

Question:

Can the CPU processing keep running when the DMAC or DTC is using the internal bus?

Answer:

If the processing requires only one bus: CPU bus, F bus, or M bus, the processing can keep running when the DMAC or DTC is using the internal bus.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211