Skip to main content
Renesas Electronics Europe - Knowledgebase

Are there PHY LSI device with a proven connection evaluation for SH721?

Latest Updated:09/09/2011


Your manual for the SH7216 has the description about connecting the SH7216 to the Ether PHY-LSI device.                                  
I wonder if there are other PHY-LSI devices with a proven connection evaluation.


The SH7216 can be connected to any PHY-LSI devices complying with MII (Media Independent Interface).
Only recognize that the necessary function and accuracy for the PHY depend on the implemented board and the usage. Please make enough advance evaluation before you decide to connect.

We offer the Application Note in "SH7216 Group Ethernet PHY Board Design Guide" as a reference on our web site. Please visit it with the following URL.
Suitable Products
SH7214, SH7216