Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is the frequency of the maximum dot clock for image output?

Latest Updated:05/06/2016

Question:

What is the frequency of the maximum dot clock for image output?

Answer:

  • The LVDS interface supports dot clocks up to 148.5 MHz. Please use a panel that supports single link. (RZ/G1N, RZ/G1M)
  • DRGB digital output supports up to 100 MHz. (RZ/G1E, RZ/G1N, RZ/G1M) 
Suitable Products
RZ/G