Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are the DDR memory types and data rates supported by the RZ/G1E and the RZ/G1M?

Latest Updated:12/02/2015

Question:

What are the DDR memory types and data rates supported by the RZ/G1E and the RZ/G1M?

Answer:

The supported DDR memory types and data rates are as follows.
RZ/G1E: DDR3 @1333 Mbps 32-bit x 1
RZ/G1M: DDR3L @1333/1600 Mbps 32-bit x 2

Suitable Products

RZ/G1E
RZ/G1M
  • Was this article helpful?