Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Supported Encoder-I/F for RZ/T1

Last Updated:09/27/2017

Question:

What kind of Encoder-I/F are supported for RZ/T1?

Answer:

At this time (August 2017), A-format™, EnDat2.2, BiSS®-C, FA-CODER® are supported, and HIPERFACE DSL® is currently under development.
Suitable Products
RZ/T1
  • Was this article helpful?