Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does the DDR interface (DDRI/F) of the RZ/G1E support 16-bit?

Latest Updated:05/09/2016

Question:

Does the DDR interface (DDRI/F) of the RZ/G1E support 16-bit?

Answer:

Yes. When using 16-bit, please connect DRAM to DRAM0 (M0DQ0 to 15).
Suitable Products
RZ/G1E
  • Was this article helpful?