Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Will an overrun error occurs when 2 frames run and 4 frames are set in SPFC?

Latest Updated:06/10/2013

Question:

When four frames are set in SPDCR.SPFC and a receive buffer full interrupt occurs, if by mistake only two frames are read instead of four, will an overrun error occur?

Answer:

Yes, an overrun error will occur.
Suitable Products
RX62N, RX621
RX62T
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111