Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

RX Family - Using Multiple Interrupts

Last Updated:06/08/2017

Question:

How do I use multiple interrupts?

Answer:

Renesas provides an application note regarding the use of multiple interrupts. See the application note "RX Family: Using Multiple Interrupts” (R01AN1954).
Suitable Products
RX Family