Skip to main content
Renesas Electronics Europe - Knowledgebase

Optimization for network connectivity and HMI function

Last Updated:11/13/2017


It is said that network connectivity and HMI function have been optimized. Which field is this optimization for? What can be realized by this optimization?


Renesas has optimized the new RX65N/RX651 MCUs for connected industrial environments.
The new MCUs offer network connectivity and HMI support that makes it possible to:

o Monitor the operating state of machinery from both inside and outside the factory
o Exchange data for making changes to production instructions
o Reprogram the MCU’s memory to update equipment settings

Suitable Products
RX65N, RX651
  • Was this article helpful?