Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it OK to use the vendor and product ID for USB task on microcontroller?

Latest Updated:12/18/2013

Question:

Is it possible to use the vendor ID and product ID obtained by Renesas for the USB function on an RX microcontroller?
Also, are the above IDs included in the free version of the USB firmware?

Answer:

Renesas does not carry out an allocation service for vendor and product IDs. Please obtain IDs from the USB Implementers Forum yourself for your end product.
Also, in the free version of the USB firmware, the value 0x0000 is set with the assumption that it will be changed by the user.
Suitable Products
RX62N, RX621
RX630
RX63N, RX631