Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to enter deep software standby mode?

Latest Updated:06/20/2013

Question:

I cannot enter deep software standby mode.

Answer:

The deep standby cancel flags in the deep standby interrupt flag register (DPSIFR) may be set to 1 when a cancel request is generated, even when not in deep software standby mode.
To enter deep software standby mode, set each deep standby cancel flag to 0 (no cancel request is generated).

For details, see Deep Standby Interrupt Flag Register (DPSIFR) and Flowchart to Use Deep Software Standby Mode in the Low Power Consumption chapter of the user's manual: hardware.

Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
  • Was this article helpful?