Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Frequency multiplication settings of the PLL clock after reset?

Latest Updated:06/26/2013

Question:

What are the frequency multiplication settings of the PLL clock after reset?

Answer:

After reset, the system clock control register (SCKCR) is initialized to 02020200h. Therefore, the system clock (ICLK), external bus clock (BCLK), and peripheral module clock (PCLK), are set to the oscillation frequency × 2 (times two).

For the initial value of SCKCR, please refer to the Register Descriptions in the Clock Generation Circuit chapter of the hardware manual.

Suitable Products
RX62N, RX621
RX610