Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Through-current when intermediate voltage is input to pin

Last Updated:01/16/2018

Question:

Does through-current flow when an intermediate voltage is applied to a Schmidt input pin ?

Answer:

In this case, through-current may flow.
Check the electrical specifications described in the relevant user's manual and use these MCUs within the specified range.
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/D1A