How to operate vector interrupt with the main clock?
Last Updated:12/26/2017
Question:
Is it necessary to input an instruction that makes the CPU clock the main clock at the beginning of the vector interrupt to operate the vector interrupt with the main clock?
Answer:
It is necessary to start oscillation of the main clock after releasing from the standby (STOP / HALT) mode.
After the oscillation stabilizes, you have to switch to the main clock.
After the oscillation stabilizes, you have to switch to the main clock.
Suitable Products
RL78 Family |
78K Family |