Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

About reference voltage of A/D converter

Last Updated:01/16/2018

Question:

For the A/D converter, can 10-bit resolution be used when the internal reference voltage (1.45V) is selected?

Answer:

As indicated in the electrical specifications in the relevant user's manual, use 8-bit resolution when the internal reference voltage (1.45V) is selected as the reference voltage of the A/D converter.
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/G13
RL78/G14
  • Was this article helpful?