Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

About RAM-ECC function support by general purpose register

Last Updated:01/16/2018

Question:

Do the general purpose registers (FFEE0H-FFEFFH) support the RAM-ECC function?

Answer:

No, the registers do not support the RAM-ECC function.
Suitable Products
RL78/F13
RL78/F14
RL78/F15