Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which has the higher priority, task 0x01 or task 0x02 ?

Latest Updated:12/01/2011

Question:

Which has the higher priority, task 0x01 or task 0x02 ?

Answer:

The smaller the value, the higher the priority (0x01 is higher in this case).
Suitable Products
  • Was this article helpful?