Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is the "intstk" stack only used for the interrupt handler?

Latest Updated:12/01/2011

Question:

The size of "intstk" is specified in the configuration file.
Is this stack only used for the interrupt handler?

Answer:

This is used for the interrupt handler and timer handler.

 

Suitable Products