Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it needed to make start address a multiple of 4 to link RX850 Pro?

Latest Updated:12/01/2011

Question:

Is it necessary to make the start address a multiple of 4 to link the RX850 Pro?
Are there any other limitations?

Answer:

As long as the start address is multiple of 4, it is OK.
There are no other limitations.
Suitable Products