Skip to main content
Renesas Electronics Europe - Knowledgebase

How many clocks does it take to perform DI?

Latest Updated:12/01/2011


Is there any processing other than using the clock handler to perform DI, such as using an OS system call?
In this case, how many clocks does it take to perform DI ?


DI processing is performed in various places within the OS such as task scheduling.
However, it is generally expressed in units of time limited to the CPU and operating clock (not calculated by the number of clocks).
Suitable Products