Skip to main content
Renesas Electronics Europe - Knowledgebase

Conditions of the HALT status is entered other than memory shortage

Latest Updated:12/01/2011


Control shifts to the initial block of the nucleus and the HALT status is entered.
Are there any conditions under which this will happen other than memory shortage?


The OS enters the HALT status when a management table cannot be created for some reason, rather than due to memory shortage.
In addition, check to make sure there is no program lockup or memory error.
Suitable Products