Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which is the pin 1 mark on the surface of the chip?

Latest Updated:08/01/2005

Question:

On the surface of the chip I can see circular white markings and stamp depressions: which is the pin 1 mark?

Answer:

The double circle is the pin 1 index. Painted markings or laser markings indicate that the product is lead (Pb) free.
Suitable Products
  • Was this article helpful?