Skip to main content
Renesas Electronics Europe - Knowledgebase

Which case is oftenly used in L level H level and high impedance result?

Latest Updated:12/01/2011


If a microcontroller port is damaged, I believe that there are cases when the L level, H level, and high impedance result, but which case is the most frequent?


This depends on the usage method, so it is not possible to tell which case is the most frequent.
Suitable Products
RL78 Family
78K Family
  • Was this article helpful?