Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What indicates EMC (Electro Magnetic Compatibility)?

Latest Updated:08/01/2005

Question:

EMC (Electro Magnetic Compatibility)

Answer:

Indicates compatibility of an electromagnetic environment.
If a current intermittently flows inside an operating electric system, noise is generated, affecting the other electric systems and causing them to malfunction.
This is considered as deterioration of the electromagnetic environment, and EMC is used to prevent this from happening.
Suitable Products