Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Public Device Address for products with Bluetooth low energy technology

Last Updated:02/13/2017

Question:

Is an assigned "Public Device Address" required to sell products with Bluetooth low energy technology?

Answer:

If using a "Random Device Address", the "Public Device Address" is not absolutely necessary. However, care should be taken because the "Random Device Address" may be duplicated possibly causing undesired operation.
Suitable Products
RL78/G1D
Bluetooth
  • Was this article helpful?