Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Bluetooth Certification for Products with RL78/G1D module (RY7011)

Last Updated:09/20/2017

Question:

How do I acquire Bluetooth certification for products equipped with the RL78/G1D module (RY7011)?

Answer:

For details on how to acquire Bluetooth certification for products equipped with the RL78/G1D module (RY7011), please refer to "3. Registration as a derived product" of the following document.

In this document, please update the following wording:

・ "RTK0EN0002C01001BZ" → "RY7011A0000DZ00"
・ "QD ID:66133" → "QD ID:82194"

Reference document:
 RL78/G1D Bluetooth certification acquisition (R01AN3177)
 https://www.renesas.com/search/keyword-search.html#q=R01AN3177&genre=document

Suitable Products
RL78/G1D
Bluetooth