Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Bluetooth SIG Qualification Significance

Last Updated:02/13/2017

Question:

What are the consequences of taking a product to market without Bluetooth SIG Qualification?

Answer:

All products must obtain Bluetooth SIG Qualification and be registered with the Bluetooth SIG in order to use the Bluetooth logo. Without completing these steps, use of the Bluetooth logo is not permitted. Any such use may fall under patent, copyright, trademark infringement, etc. Please direct further questions to the Bluetooth SIG.
Suitable Products
RL78/G1D
Bluetooth