Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What to use: GDB Hardware Debugging or Renesas GDB Hardware Debugging

Latest Updated:12/09/2014

Question:

There are two debug configurations: "GDB Hardware Debugging" and "Renesas GDB Hardware Debugging."  Which should I use?

Answer:

"Renesas GDB Hardware Debugging" is applicable for Renesas device, while "GDB Hardware Debugging" is a configuration for standard eclipse plugin.
Suitable Products
e² studio