Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Specifying linkage order in e² studio

Last Updated:05/24/2017

Question:

How can I specify linkage order in e² studio?

Answer:

From the project property, go to “Linker”, “Input”, and then “Advanced”. Select the “Use custom linkage order” check box.

This allows you to set the linkage order of objects.

Suitable Products
e² studio
  • Was this article helpful?