Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Meaning of outlined font icons for source files(e² studio)

Last Updated:08/09/2017

Question:

In e² studio project, why some source file icons have outlined font, while others do not?

Answer:

Regular font icons, such as ".C" and ".H", indicate files which are recognized as build target source code or headers located in the include path of a project.

Conversely, files shown as outlined font icons are excluded from build target, or out of the include path.

For example, if only the files in the /src folder of a project are specified as build targets, the icons of files outside the /src folder have outlined font. Therefore, they are recognized as being excluded from the build target.

By moving source files into /src, the icon will change to normal, and then be accepted as build target.

If you wish to configure a build target folder, refer to the following FAQ page.

FAQNo:1011347
Why source file cannot be found in <project folder>/src,?

Suitable Products
e² studio