How to overwrite existing program when downloading to flash memory?
Latest Updated:12/11/2014
Question:
How can I overwrite existing program when downloading a program to the flash memory?
Answer:
In default configuration of the hardware debugger setting, program is downloaded into flash ROM after erasing the ROM.
Please change the setting with the following steps:
- select Debug Configuration View from debug button or Run menu to open a dialog,
- select target configuration in the left tree view,
- select "Debugger" tab -> "Connection Settings" -> Flash, and
- change "Erase Flash ROM When Starting" from "Yes" to "No."
Suitable Products
e² studio |