Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How can I change the build output format?

Latest Updated:12/15/2014

Question:

How can I change the build output format?

Answer:

You can change the format with "RenesasToolSettings" of a project in the following steps:

  1. Open the property dialog by either of the following procedures:
    • Start the project explorer and focus on a project name and select "Property" by right-click.
    • Press [Alt]+[Enter] or [Alt]+[T].

  2. Click “C/C++ Build” option to display the setting of configuration and edit each format.

    [compiler output format (*.obj as default)]
    "Renesas Tool Settings" (Alt+T) -> "C/C++ Build" -> "Compiler" -> "Object" -> "Output file type"
    [linker output format (*.mot/*.x as default)]
    "Renesas Tool Settings" (Alt+T) -> "C/C++ Build" -> "Linker" -> "Output" -> "Type of output file:"

 

Suitable Products
e² studio