Q0140035 Message_CS+
Last Updated:12/20/2017
Question:
When I tried to use the integrated uninstaller of the CS+ integrated development environment, the Q0140035 message appeared. What should I do about the message?
Answer:
When the rapid start function of CS+ is enabled, CS+ stays resident for improved startup speed. Right-click on the CS+ icon in the notification area (system tray) and select [Exit] to terminate CS+. Then, use the integrated uninstaller.
Suitable Products
CS+ (formerly CubeSuite+) |