Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

My security software indicated the CS+ file as a threat

Last Updated:02/21/2017

Question:

My security software indicated the CS+ integrated development environment installation file as a threat. I don’t think it is likely, but could it have malware?

Answer:

To ensure the CS+ installation file are free of viruses & malware, we use Forefront Endpoint Protection from Microsoft Corporation to verify the CS+ installation file is clean.

If necessary, instruct the security software to allow the CS+ installation to execute.

Suitable Products
CS+ (formerly CubeSuite+)