Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is the RL78 C compiler license bought with CS+ valid for e² studio, too?

Latest Updated:09/04/2015

Question:

Is the RL78 C compiler license bought with CS+ valid for e² studio, too?

Answer:

RL78 C compilers having the major version number 1.X which are included in a CS+ package can be integrated into e² studio using the current license.

For example, if the compiler supplied with CS+ was V1.01.00, then all V1.X RL78 C compiler versions (e.g. V1.01.00, V1.02.00, ...) can be integrated into e² studio using the current valid licenses.

How to add toolchain:
To use CS+ toolchain,

  1. Press toolbar button of "Integrate non-integrated toolchain" to open "Renesas Toolchain Management" view.
  2. Check desired toolchain(s).
    If desired product(s) were not listed, press [Add] button and specify the installed location.

CC-RL in CS+ toolchains is typically at this location:
C:/Program Files/Renesas Electronics/CS+/CC/CC-RL/(version number)

Note 1: The "C Compiler for RL78 and 78K Families" of CubeSuite+ is not applicable for e² studio.

icon_diverge.gifNote 2: This FAQ is subjected to be applied to Asian area license distributions.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family