Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to use English of CS+, Renesas Flash Programmer, & PG-FP5

Last Updated:06/14/2017

Question:

I would like to use the English versions of CS+, Renesas Flash Programmer, and PG-FP5.

Answer:

There is no distinction between the Japanese and English versions of CS+, the Renesas Flash Programmer, and the programming GUI for PG-FP5.
English text is automatically displayed when they are installed on a PC with an OS other than a Japanese version.
Suitable Products
CS+ (formerly CubeSuite+)
PG-FP5
Renesas Flash Programmer
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family