Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to resolve if I got an error xxxx.rel using CC-RL compiler RL78?

Latest Updated:07/14/2015

Question:

I am using the CC-RL compiler for RL78 devices. I get the error message below when I designate an object file as an input file. How do I resolve this?

E0562200: Illegal object file : "xxxx.rel"

Answer:

Check that you have not designated an object file for CA78K0R. You cannot use the CC-RL compiler to link an object which was generated with CA78K0R because they are in different object formats. Please recreate the object file for CC-RL.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family