Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to prevent a project from being automatically loaded at startup (CS+ Integrated Development Environment)

Last Updated:06/07/2017

Question:

I am using the CS+ integrated development environment.

A project seems to be automatically loaded at startup of CS+. Is there any method to prevent a project from being automatically loaded?

Answer:

In CS+, a function to automatically load the project that was in use at the time of the last termination is enabled by default.

To enable or disable this function, select the [General - Startup and Exit] category in the Option dialog box, and then select or clear the [Load the last project at CS+ startup] check box.

For details about the [General - Startup and Exit] category in the Option dialog box, see this site.

Suitable Products
CS+ (formerly CubeSuite+)
  • Was this article helpful?